The Apply of AMCLIB_BemfObsrvDQ and AMCLIB_TrackObsrv in MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The Apply of AMCLIB_BemfObsrvDQ and AMCLIB_TrackObsrv in MPC5744P

352 Views
Edison_LI
Contributor II

Hi,

I used the AMCLIB_BemfObsrvDQ and AMCLIB_TrackObsrv in my project for the sensorless control,when it doesn't enter into the sensorless mode,the speed and angle that observed is very good and stable.

However, once it enter into the sensorless mode ,the speed would be a large negative value, and the motor would spin rapidly in the opposite direction for a few turns and then stop.

The version of MPC574xP_AMMCLIB I used is 1.1.15

I‘m not sure what the problem is. Can you give me some advice

 

Best regard

Edison.Li

0 Kudos
Reply
0 Replies