I have purchased TRK-MPC5606B Development Board, Along with that I got a Sample code named "Training_LED_Example" and some documents giving directions for programming, Hardware layout, connections, etc.
I got a pdf "FSK_TRK_MPC5606B_Training" along with the development board, in which they have explained connections and basics about the "Training_LED_Example" program.
But I couldn't find any document, PPT, Video or tutorial in which I can get to know about How to debug the program and check the register values/status etc?
Please help me to understand how to debug the code on TRK-MPC5606B Board (using JTAG or by some other mean please)
Thanks in advance.
-Akshay P Daga
hi
this video is helpful in starting codewarrior and debugging it
when watching it while selecting microcontroller select the one you are using.
CodeWarrior Intro Create a Project and Debug Watch in HD - YouTube
Hi,
if you use CodeWarrior 2.10, see this document:
c:\Program Files\Freescale\CW for MPC55xx and MPC56xx 2.10\Help\PDF\ICDPPCNEXUS Quick Start Guide.pdf
if you use CodeWarrior 10.6, see:
c:\Freescale\CW MCU v10.6\MCU\Help\PDF\CodeWarrior Common Features Guide.pdf
You can find other SW examples here:
or in AN2865:
http://www.nxp.com/files/32bit/doc/app_note/AN2865.pdf
MPC5500 and MPC5600 Simple Cookbook Code
Lukas
It is always a good idea to start with documentation of your EVB, maybe AN4850 will help:
I have gone through the document AN4850. But Doen't give any idea about checking Internal register status/value or Debugging the project created in CodeWarrior directly.
How to develope code for debugging in free master is not given in there.
(It gives idea only about the sample code created in RAppID tool and then ported into codeWarrior using CWPJMaker and then checking the values of the variables on FreeMaster)
I can see, there is debug option available in codewarrior itself, Please help me to use that option.
Thanks.
CodeWarrior Development Studio
-CodeWarrior for MCU
Version: 10.5
Build ID: 130916