TJA1100 with SPC58NG84E7 is not working, all configurations are made correctly but the Link_UP bit is not set correctly?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1100 with SPC58NG84E7 is not working, all configurations are made correctly but the Link_UP bit is not set correctly?

641 Views
mahmoud_abdelka
Contributor I

we are using the TJA1100 transciver with SPC58NG84E7, all configuration registers are set correctly according to the data sheet and the application note, all the bits in the status registers are as expected except for the REM_RCVR_STATUS and the LINK_UP, i also tried to connect my board to other Rx devices and different cables and the same result, i also swapped between master and slave mode and still the same porblem. i attach below my PHY registers values

reg[0]0x4006C51C0x2120
reg[1]0x4006C5200x1E5
reg[2]0x4006C5240x180
reg[3]0x4006C5280xDC41
reg[15]0x4006C5580x80
reg[16]0x4006C55C0xA9
reg[17]0x4006C5600x9806
reg[18]0x4006C5640xD818
reg[19]0x4006C5680x2245
reg[20]0x4006C56C0x0
reg[21]0x4006C5700x4040
reg[22]0x4006C5740xFFFF
reg[23]0x4006C5780x3024
reg[24]0x4006C57C0x6200
reg[25]0x4006C5800x20
reg[26]0x4006C5840x0
Tags (2)
0 Kudos
Reply
1 Reply

606 Views
Bulat
NXP Employee
NXP Employee

Registers show that the PHY was successfully initialized and can not establish link with a remote partner. Typically this relates to problems with cable connections or MDI circuitry shown in figure 17 of the TJA1100 data sheet.

Regards,

Bulat

0 Kudos
Reply