TJA1100 : When SSD_ERR and RECEIVE_ERR bits would be set?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TJA1100 : When SSD_ERR and RECEIVE_ERR bits would be set?

945 Views
sukruthrameshba
Contributor III

Hi,

Under what scenarios will the SSD_ERR and RECEIVE_ERR will be set in Communication Status register (Register 23) of TJA1100 , ? It would be of great help if this could be explained in detail.

Regards,

Sukruth

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

880 Views
Bulat
NXP Employee
NXP Employee

This basically comes from IEEE 802.3 specifications. Please take a look at receive state diagrams in section 96.3.4.1. SSD_ERR is set if the state machine gets to state "BAD SSD" (figure 96-10a). RECEIVE_ERR is set in case of  state "RX ERROR" (figure 96-10b).

Regards,

Bulat

0 Kudos
Reply