TJA1100 : When SSD_ERR and RECEIVE_ERR bits would be set?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1100 : When SSD_ERR and RECEIVE_ERR bits would be set?

550件の閲覧回数
sukruthrameshba
Contributor III

Hi,

Under what scenarios will the SSD_ERR and RECEIVE_ERR will be set in Communication Status register (Register 23) of TJA1100 , ? It would be of great help if this could be explained in detail.

Regards,

Sukruth

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

485件の閲覧回数
Bulat
NXP Employee
NXP Employee

This basically comes from IEEE 802.3 specifications. Please take a look at receive state diagrams in section 96.3.4.1. SSD_ERR is set if the state machine gets to state "BAD SSD" (figure 96-10a). RECEIVE_ERR is set in case of  state "RX ERROR" (figure 96-10b).

Regards,

Bulat

0 件の賞賛