Some possible bugs in S32_SDK_MPC574xx_RTM_1.0.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Some possible bugs in S32_SDK_MPC574xx_RTM_1.0.0

跳至解决方案
549 次查看
shanix
Contributor II

Hello

When I use the S32_SDK_MPC574xx_RTM_1.0.0 on the MPC5748G, I found some code in SDK that may be problematical and would like to have it confirmed. Thanks.

shanix_0-1694400455999.pngshanix_1-1694400463453.png

 

 

0 项奖励
1 解答
492 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you have quite old SDK version, I can recommend to use the latest one, below is snippet from RTM 3.0.3

 

2023-09-11_12-13-32.png

Yes, setting of WRNEN is possible in Freeze mode only. 
A driver enable error interrupts if you install error callback using FLEXCAN_DRV_InstallErrorCallback, and Freeze mode is entered in it.

BR, Petr

在原帖中查看解决方案

0 项奖励
3 回复数
493 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you have quite old SDK version, I can recommend to use the latest one, below is snippet from RTM 3.0.3

 

2023-09-11_12-13-32.png

Yes, setting of WRNEN is possible in Freeze mode only. 
A driver enable error interrupts if you install error callback using FLEXCAN_DRV_InstallErrorCallback, and Freeze mode is entered in it.

BR, Petr

0 项奖励
489 次查看
shanix
Contributor II
Thanks! Your reply is very useful. Maybe I need to migrate to the new verison SDK.
0 项奖励
516 次查看
shanix
Contributor II

shanix_0-1694419453801.png

 

0 项奖励