I have two sensor communicate with DSPI0 with two chip select. One chip select works what I expect. But second chip select do not work properly. I think second pin may be crush or something and I change the second chip select's pin. I try four chip select pin for this purpose and I see only first one works. I do not understand why this happen. Is this problem cause for software or hardware I do not know actually.
First chip select PCSA0(it works):
Second chip select PCSA1(it does not work; interestingly chip select's reset state around 0.4V (I expect 5V)):
PCSA2: I do not use this pin because I do not see this pin in my motherboard
PCSA3(this pin does not work): When I select this pin as a second chip select This pin always in low state (0V):
PCSA4(this pin does not work but it has interesting output): When I select this pin as a second chip select it does not work and generate interesting output:
PCSA5(it does not work): When I select this pin as a second chip select This pin always in low state (0V):
By the way I use this motherboard:
And Which information I use for determine the chip select pins:
And lastly I want to share with you what configuration I did about software:
Solved! Go to Solution.
They are jumper for ethernet PHY on these pins (routed to motherboard). Check them, whether you have them in place or not.
They are jumper for ethernet PHY on these pins (routed to motherboard). Check them, whether you have them in place or not.