Safety certification for the gcc compiler in S32DS for power architecture devices

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Safety certification for the gcc compiler in S32DS for power architecture devices

1,497 次查看
AndrewwDabach
Contributor II

Hi,

 

I am working with MPC5744P with the e200z4 processors. I am using the S32DS version 2.1 with the integrated NXP gcc comiler v4.9. I am interested in the safety certifications of the IDE and the compiler as well?

 

Thanks in advance

0 项奖励
回复
5 回复数

1,463 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

S32DS is according the ASIL-D:

The performed tool classification determined the qualification need of the used tools, and is
based on the use cases of the tools and the safety standard requirements (tool classes). The
classification was completed according to ISO 26262, with the maximal level ASIL D.

GCC compiler is not safety certified.

For such please use GHS or IAR.

Sharing of any safety documents can be done only via support tickets at NXP.com

Best regards,

Peter

0 项奖励
回复

1,458 次查看
AndrewwDabach
Contributor II

Hi,

Thank you for your response. Although IAR doesn't support power architecture, I will check with GHS. Additionally, could you also provide me information about the safety certification of the SDK provided for the same MCU MPC5744P?

Thank you

0 项奖励
回复

1,438 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

There is no safety for SDK for this device.

You can use MCAL ISO26262 package which is ASIL-D certified.

Best regards,

Peter

0 项奖励
回复

1,435 次查看
AndrewwDabach
Contributor II

Hi,
Thank you for your response. Could you please let me know where can I find the "MCAL ISO26262 package"? Additionally, is the "Processor Expert" tool and code generated from the tool are safety certified ?

Thank you

0 项奖励
回复

1,417 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Here is the link for MCAL:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW574XP-SMCL401E

Additionally, is the "Processor Expert" tool and code generated from the tool are safety certified ?

Whole S32DS classification was completed according to ISO 26262. Including configuration tool.

External tools like compilator is not as it is supplied by third party so user can choose which one fits their application the most.

You can also have a look at windriver they also support safety compiler.

Best regards,

Peter

0 项奖励
回复