SPC5746 Device Pinout and Package Information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5746 Device Pinout and Package Information

3,685 Views
daveschaefer
Contributor II

Pinouts in the attached excel spreadsheet of the MPC5746CRM.pdf for "BGA256" do not match supplied NXP mechanical drawing Document No: 98ASA00468D Rev.A "MAPBGA, LOW PROFILE, 17 x 17 x 1.54 PKG, 0.8 MM PITCH, 252 I/O".

 

Where can I obtain the correct mechanical package and pinout information for this device?

Labels (1)
0 Kudos
1 Reply

1,358 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

first of all, SPC5746R is covered by this datasheet:

http://www.nxp.com/files/32bit/doc/data_sheet/MPC5746R.pdf

… and reference manual:

http://www.nxp.com/files/32bit/doc/ref_manual/MPC5746RRM.pdf

It’s not MPC5746CRM.pdf because SPC5746R and SPC5746C are two different devices.

 

SPC5746RK1MMT5 has 252 MAPBGA package and the drawing is:

http://www.nxp.com/files/shared/doc/package_info/98ASA00468D.pdf

The description of pinout can be found in excel sheet which is attached to the reference manual (link above).

Regards,

Lukas

0 Kudos