We have for your company's SPC5634MF1MLQ80 TQFP144 microcontroller in burning program, through a number of times there are some material software don't burn in!
Has not been tried two ways respectively, burn write success
Using CodeWarrior IDE v2.10 and OSJTAG debugger to burn (interface such as attachment 1)
USES MPC chip bringing the Bootloader program written BDM mode, through RS232 burning (burning failure interface as shown in attachment 3), RS232 model for: TEK ZE551A
我司在对贵司的SPC5634MF1MLQ80,TQFP144单片机烧录程序时,通一批次其中有部分物料软件烧录不进去!
分别尝试了两种方式,均未烧写成功
采用CodeWarrior IDE v2.10和OSJTAG调试器进行烧录(失败界面如附件1)
采用MPC芯片自带的BDM模式编写的Bootloader程序,通过RS232烧写(烧写失败界面如附件3所示),RS232型号为:TEK ZE551A
以上异常请协助分析什么原因。谢谢!
The above abnormal please help analysis the reason why.Thank you very much!