SPC5607B SWT Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPC5607B SWT Problem

2,248件の閲覧回数
yankuang1
Contributor III

Hi ,

I set the timeout reset time of SWT to 10s, and when I enable the interruption, SWT can normally reset after 10s timeout and F_CHECKSTOP set.

But if the interrupt is not turned on, 20s is needed before resetting. The resetting register is F_SOFT. Please help to check why this situation occurs.

0 件の賞賛
返信
1 返信

2,153件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

reference manual:

pastedImage_2.png

If the interrupt is not enabled the device will be reset after 10s

If it is enabled and not SWT in not updated in interrupt it will reset on second timeout. 20s

regards,

Peter

0 件の賞賛
返信