SPC5606BF1MLQ6 replace ST SPC560B50L5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPC5606BF1MLQ6 replace ST SPC560B50L5

Jump to solution
1,016 Views
ZhaozhangChen
Contributor I

Dear Support,

I have a project based on ST SPC560B50L5 design schematic and software. Now we need to replace ST SPC560B50L5 with NXP SPC5606BF1MLQ6, but I found that the 81 and 82 pins of NXP SPC5606BF1MLQ6 LQFP 144 PIN package are different from ST SPC560B50L5. And the design uses these two pins as ADC acquisition ports. Could you please help confirm whether NXP SPC5606BF1MLQ6 can replace ST SPC560B50L5 and whether the software and hardware are compatible? Thank you!

ZhaozhangChen_1-1655887949228.png

ZhaozhangChen_2-1655888222506.png

 

 

 

 

0 Kudos
1 Solution
1,005 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is because these are two different families

ST number SPC560B50L5 is equivalent to MPC5604B, covered by following RM:
https://www.nxp.com/webapp/Download?colCode=MPC5604BCRM

SPC5606BF1MLQ6 belongs to MPC5607B, covered by:
https://www.nxp.com/webapp/Download?colCode=MPC5607BRM

There is an appnote describing differences between MPC5607B and MPC5604B families:
https://www.nxp.com/docs/en/application-note/AN4340.pdf

 

View solution in original post

6 Replies
1,006 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is because these are two different families

ST number SPC560B50L5 is equivalent to MPC5604B, covered by following RM:
https://www.nxp.com/webapp/Download?colCode=MPC5604BCRM

SPC5606BF1MLQ6 belongs to MPC5607B, covered by:
https://www.nxp.com/webapp/Download?colCode=MPC5607BRM

There is an appnote describing differences between MPC5607B and MPC5604B families:
https://www.nxp.com/docs/en/application-note/AN4340.pdf

 

964 Views
ZhaozhangChen
Contributor I

I want to replace ST SPC560B50L5C6E0Y with NXP SPC560B50L5C6E0Y to produce BCM products. The firmware of the product is ST SPC560B50L5C6E0Y. Can I use the firmware directly on NXP SPC5604BAMLQ6? Thanks

0 Kudos
960 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It could work unless mentioned differences are not an issue. MPC5607B peripherals are backward compatible with MPC5604B.

Also SW should not check Device ID as this numbers are different.

0 Kudos
957 Views
ZhaozhangChen
Contributor I

Sorry, I did not give a clear description. My question is whether the firmware of ST can be compatible with the operation of NXP .

0 Kudos
945 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I don't have any information about ST device, according to my knowledge it should be equivalent to MPC5604B, but they may differ in used mask, revisions. I can give you only info about NXP devices.

User SW may test SIU_MIDR2 register where they may be a difference in revisions or manufacturer field.

0 Kudos
1,003 Views
ZhaozhangChen
Contributor I

Thank you very much for your help

0 Kudos