Is your problem solved? , How to look at the data from the ram, I have the starting address of the ADC, but the data seems wrong
Hi,
I am not SD ADC expert, but from my point of view, it is not possible to read output data from SD ADC directly. This data are provided to ACQ (A-H) unit, which is also part of Acquisition Block, which executes complex mathematical operation with the data.
If you only need analog to digital conversion without the features of Signal Processing Toolbox, I can recommend you SAR-ADC, which is determined for this purpose.
Regards,
Martin
Hi Martin, very thanks for your reply! However, I don't know the function of the ACQ(a-h), and i'm not sure how the data is changed after this unit . And i just know the sample data is transfered to systerm RAM via the SDMA ,so now i want to read the data from systerm ram , but it's difficult for me .Do you know how to solve this problem?
Besides, I need the ADC works at 10Ms/sec ,so i can't use the SAR-ADC for its low sample rates but the SD-ADC in AFE.
Hi,
ACQ is only a small part of the SPE module, which is very complex. I am not able to tell you, how to use it, because it is out of my scope. Unfortunately, I am not able to provide any document or application note how to work with this module.
The only possibility how to get the information about this modules is professional support.
Professional Support for Microcontrollers|NXP
Regards,
Martin
i'm looking forward to your reply~
and my email address : tian9496@foxmail.com