S32R274 RSDK Demo Project based on GreenHills compiler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R274 RSDK Demo Project based on GreenHills compiler

532 Views
Durant-Harden-Irving
Contributor III

Dear,

Question background:

Step1: I had install the S32R_DS_Project, and generated the projects "RSDK_Demo_Z4_0" and "RSDK_Demo_Z7_1" .

Step2: Then I build the project, and download to RSDK, it works well

Step3:I would like to use the GreenHills V7.1.6  compiler to build projects "RSDK_Demo_Z4_0" and "RSDK_Demo_Z7_1", I found the porting workload is large.

Question:

Do you have the projects based on GreenHills compiler? (the project features is similar to projects "RSDK_Demo_Z4_0" and "RSDK_Demo_Z7_1", including clock init & interrupt init & SPT process & Ethernet... ) 

Thanks very much!

MF
0 Kudos
2 Replies

500 Views
Durant-Harden-Irving
Contributor III

Also thanks!

MF
0 Kudos

512 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Unfortunately no, RSDK is supported only if S32DS.

best regards,

Peter

0 Kudos