Hello, everyone, please ask a question. When I created the NXP5748G flashDrv RAM, I wanted to generate a position-independent code base. But I use S32 Design Studio for Power Architecture Version 2.1 to create an application project, this ld configuration option -nostartfiles does not work? Does anyone know how to configure and modify the ld file option?
Application Project Properties: Standard S32DS C/C++ Linker > General
thanks!
Hi,
the -nostartfiles option tells the linker to do not use startup from STD C library. But you still need to use some startup to configure your MCU.
Jiri
Hi, there is an example for PIC, however for different platform.
I will check whether PIC example for S32DS for Power exists.
thanks! old project use 5744P and S32 Design Studio for Power Architecture Version 2017.R1 import S32 Design Studio for Power Architecture Version 2.1,create map file
.startup 0x40030400 0x0
0x40030400 __start = .
*(.startup)
But I creat new 5748G and S32 Design Studio for Power Architecture Version 2.1 , create map file
.startup 0x40030020 0x1ee
0x40030020 __start = .
*(.startup)
.startup 0x40030020 0x1ee ./Project_Settings/Startup_Code/startup.o
0x40030020 _start
0x4003020a _fini
I Does not compile the startup.S, solved this problem.Did you know that this problem can be solved by configuring or modifying the ld file?
Hi,
to be honest - I don't get it. So, can you describe in more details what you are trying to do or what's your approach?
Jiri
hi,thanks!
My purpose is to use S32 Design Studio for Power Architecture Version 2.1 to compile the C55_JDP_SSD.exe flash driver file to generate a single-block *.Srec, and then use hexview.exe to export the C language array method, and put the C language array content in RAM , It is used for erasing 5748GMCU flash, but the srec file generated by my new project is multi-block. If startup.S is not compiled, a single-block can be generated.5748G SREC文件
Hi,
I do not understand why to compile the drivers again. The package already contains pre-compiled drivers either in c-array format or in s-record format. If you want to have single package of the functions, you can simply concacenate them without changes.
Regards,
Lukas
hi,We need to provide customers with a packaged flash erasing function and a separate serc format file, which is convenient for the host computer to download to the ram erasing flash, so we need to recompile the *.C file of c-array_driver to form a file, and NXP provides the driver Srec is a single file that is not convenient for customers to download.
Let me confirm if I can understand it - you just need to have our SSD drivers in single file, correct? Do you need it as single s-record file or as single c-array?
Regards,
Lukas
Hi,correct. My purpose is to use S32 Design Studio for Power Architecture Version 2.1 to compile the C55_JDP_SSD.exe flash driver *.c file to generate a single-block *.Srec for nxp 5748G.
thanks!
thanks ! The file you gave is what I need, but my starting address is 0x40030000, can you give me your project file or tell me the configuration steps to generate a single-block srec file?