S32DSforPowerV2.1's ld option -nostartfiles does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DSforPowerV2.1's ld option -nostartfiles does not work

2,941 Views
goodfriends
Contributor I

Hello, everyone, please ask a question. When I created the NXP5748G flashDrv RAM, I wanted to generate a position-independent code base. But I use S32 Design Studio for Power Architecture Version 2.1 to create an application project, this ld configuration option -nostartfiles does not work? Does anyone know how to configure and modify the ld file option?

Application Project Properties: Standard S32DS C/C++ Linker > General

thanks!

0 Kudos
Reply
12 Replies

2,905 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

the -nostartfiles option tells the linker to do not use startup from STD C library. But you still need to use some startup to configure your MCU. 

 

Jiri

0 Kudos
Reply

2,933 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, there is an example for PIC, however for different platform.

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/EXAMPLE-S32K144-Position-Independent-C...

I will check whether PIC example for S32DS for Power exists.

0 Kudos
Reply

2,929 Views
goodfriends
Contributor I

thanks!  old project use 5744P and S32 Design Studio for Power Architecture Version 2017.R1 import S32 Design Studio for Power Architecture Version 2.1,create map file

 .startup        0x40030400        0x0

                0x40030400                __start = .

 *(.startup)

 

But I creat new 5748G and   S32 Design Studio for Power Architecture Version 2.1 , create map file

.startup        0x40030020      0x1ee

                0x40030020                __start = .

 *(.startup)

 .startup       0x40030020      0x1ee ./Project_Settings/Startup_Code/startup.o

                0x40030020                _start

                0x4003020a                _fini 

I Does not compile the startup.S, solved this problem.Did you know that this problem can be solved by configuring or modifying the ld file?

0 Kudos
Reply

2,901 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

to be honest - I don't get it. So, can you describe in more details what you are trying to do or what's your approach? 

 

Jiri

0 Kudos
Reply

2,892 Views
goodfriends
Contributor I

hi,thanks!

My purpose is to use S32 Design Studio for Power Architecture Version 2.1 to compile the C55_JDP_SSD.exe flash driver file to generate a single-block *.Srec, and then use hexview.exe to export the C language array method, and put the C language array content in RAM , It is used for erasing 5748GMCU flash, but the srec file generated by my new project is multi-block. If startup.S is not compiled, a single-block can be generated.5748G SREC文件5748G SREC文件

image.png

 

0 Kudos
Reply

2,874 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I do not understand why to compile the drivers again. The package already contains pre-compiled drivers either in c-array format or in s-record format. If you want to have single package of the functions, you can simply concacenate them without changes.

Regards,

Lukas

0 Kudos
Reply

2,858 Views
goodfriends
Contributor I

hi,We need to provide customers with a packaged flash erasing function and a separate serc format file, which is convenient for the host computer to download to the ram erasing flash, so we need to recompile the *.C file of c-array_driver to form a file, and NXP provides the driver Srec is a single file that is not convenient for customers to download.

0 Kudos
Reply

2,799 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Let me confirm if I can understand it - you just need to have our SSD drivers in single file, correct? Do you need it as single s-record file or as single c-array?

Regards,

Lukas

0 Kudos
Reply

2,768 Views
goodfriends
Contributor I

Hi,correct. My purpose is to use S32 Design Studio for Power Architecture Version 2.1 to compile the C55_JDP_SSD.exe flash driver *.c file to generate a single-block *.Srec for nxp 5748G.

thanks!

0 Kudos
Reply

2,740 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at attached files. One version is generated for s-record base address 0x0, second for 0x40000000. Not sure which one is better for you. Offsets for individual functions can be found in the excel file.

Hope it helps.

Regards,

Lukas

0 Kudos
Reply

2,732 Views
goodfriends
Contributor I

thanks ! The file you gave is what I need, but my starting address is 0x40030000, can you give me your project file or tell me the configuration steps to generate a single-block srec file?

0 Kudos
Reply

2,727 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Attached. I wrote very simple script for Lauterbach debugger to load the individual files to RAM and then I saved the content of that area to s-record file with specified offset. This is much easier (from my point of view, at least) than playing with S32DS...

Regards,

Lukas

0 Kudos
Reply