S32 DS for PA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 DS for PA

2,059 Views
Jerrylh
Contributor I

I have a project of mpc5746c, when I debug ram, it has no problem, but when I debug (flash), it has one error, "run time error 216 at 043842C6".I don't know what the problem is, the development board or the project setting?

0 Kudos
Reply
3 Replies

2,043 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I never seen this issue before.

Do you have updated PE micro plugin?

Could you sent me full output from debug console and a .log file from workspace?

c:\Users\nxf24838\workspaceS32DS.Power.2.1\.metadata\ 

best regards,

Peter

0 Kudos
Reply

2,034 Views
Jerrylh
Contributor I

hello,

Thank you for your answer.Please see the attachment.

0 Kudos
Reply

2,013 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

 

the log file says -  Resource '/MPC5746C_TEST01OS_Z4_0' is not open.  The issue is related to all projects or only to this one? What about file atributes (write/read permissions)? 

 

Jiri

0 Kudos
Reply