Receiving Ethernet Frames on MPC5748G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Receiving Ethernet Frames on MPC5748G

1,160件の閲覧回数
rubik__90
Contributor II

Hello everyone,

I am a beginner and I would like to receive ethernet frames from PC to MPC5748G. I used the enet_rmii_udp example to correctly transmit from the board to PC, but I am not able to receive.

Could someone give me a suggestion?

Thanks in advance

 

0 件の賞賛
返信
2 返答(返信)

1,125件の閲覧回数
rubik__90
Contributor II

Hi,

thanks for your reply. I tried to take a look to your thread, but it doesn't work for me. No matter what type of data I'm going to send/receive, it's just a didactical exercise.

I would like to do it ease using the API included in MPC5748G_SDK_Z4_0, but it does not work simply calling "ENET_DRV_ReadFrame" and "ENET_DRV_SendFrame".  Do you think it can be done this way, editing enet_rmii_udp example?

Thanks in advance,

Antonio

0 件の賞賛
返信

1,144件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

what is the data send from PC, in fact?
Should below thread address this somehow?
https://community.nxp.com/t5/MPC5xxx/ethernet-project-of-mpc5748g/m-p/942500

BR, Petr

0 件の賞賛
返信