Hello,
I am currently trying to get SPI data transfer between the MPC5744p and a Raspberry Pi 4 to work.
I'm using the SPIdev python toolkit to send the value 26 over to the MPC, using the attached SPItest.py script.
To receive this, i've modified the code of the SPI_MPC5744P example to only expect data arriving on the slave DSPI2.
When testing this my connections were as follows:
Raspberry Pi NXP
SCLK → DSPI_2 CLK (PA0 - J5_1)
MOSI → DSPI_2_SIN (PA2 - J5_5)
The code on the MPC5744P was intended to send a message to UART when SPI transfer has happened. However, when using the script on the Raspberry Pi, I could not get this message to show up.
I'm currently stuck as I can't seem to find out what I'm forgetting?
At first I thought that i also needed to connect the Slave Select pin, but the reference manual says that you shouldn't tie this to ground?
Thank you for your time.