RSDK lib rebuilding of S32R274

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RSDK lib rebuilding of S32R274

Jump to solution
1,958 Views
Durant-Harden-Irving
Contributor III

Hello,

Now we are using GreenHills compiler, if link the RSDK libs in below folder, do I need to rebuild the RSDK code and generate new libs based on GreenHills compiler?

..\NXP\S32DS_Power_v2.1\S32DS\software\S32_SDK_S32PA_RTM_3.0.3\middleware\rsdk

Thanks!

 

MF
0 Kudos
Reply
1 Solution
1,913 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Radar team express that chances are very low to port it for GHS.

You can ask GHS, but I cant say if they have knowledge on SPT toolbox.

best regards,

Peter

View solution in original post

4 Replies
1,933 Views
Durant-Harden-Irving
Contributor III

In my opinion, the c code  modification of RSDK for the GHS is feasible.  After all we have do that for other modules, and test well.

But I am not sure, if it is feasible for the SPT kernel file(*.pspt file). 

Or, should I ask the support from GHS?

Thanks!

MF
0 Kudos
Reply
1,914 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Radar team express that chances are very low to port it for GHS.

You can ask GHS, but I cant say if they have knowledge on SPT toolbox.

best regards,

Peter

1,948 Views
Durant-Harden-Irving
Contributor III

Thanks for your reply!

If we try to build RSDK libs  by  GHS compiler, it is feasible(modify the souce code to adapt), right?

Especially for the SPT kernel file(*.pspt file), is it feasible for building by the GHS compiler ?

Thanks!

MF
0 Kudos
Reply
1,949 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

We do not support GHS compiler. We have never tried to build with it neither try to mix build RSDK libs iwth gcc and application with other compiler.

The chances are near 0.

Best regards,

Peter