RAppID and MPC5674F over CAN Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAppID and MPC5674F over CAN Error

537 Views
czechu82
Contributor II

Hello,

I try to read out MPC5674F over CAN but getting an error "Lost communication with CCP MCU...."
Using CANCaseXL, Vector hardware enabled, baud rate set to 250k.
Connection is ok since i can see all CAN messages with BUSMASTER.

Does MPC5674F support CAN connection ?

Here are logs from Trace output window:

TX:      011    01 00 00 00 AA AA AA AA 
RX:     001    00 00 00 00 00 00 00 00       TX:      011       01 00 00 00 AA AA AA AA 
RX:     001    00 00 00 00 00 00 00 00          Init
TX:      011    01 00 00 00 AA AA AA AA 
RX:     001    00 00 00 00 00 00 00 00       TX:    011       01 00 00 00 AA AA AA AA 
RX:     001    00 00 00 00 00 00 00 00          Init

Thank You.

1 Reply

423 Views
czechu82
Contributor II

also tried 500k