Hi.
I try to enable FEC with MII interface setting, but nothing works so far.
I used 'AN4577_Using the Fast Ethernet Controller on the Qorivva MPC564xBC' document as a reference.
There are three questions about
1. FEC I/O setting
2. FEC Clock setting
3. isConnected() function (miiRead function)
Questions are below
1. FEC I/O setting - please check I/O setting
#define OBE 0x0200
#define IBE 0x0100
#define ODE 0x0020
#define SRC 0x0004
#define WPE 0x0002
#define WPS 0x0001
#define PA_GPIO 0x0000
#define PA_PRIM 0x0400
#define PA_ALT1 0x0800
#define PA_ALT2 0x0C00
#define PA_ALT3 0x1000
// initFecIo - initialise pads for FEC use in the SIU
void initFecIo(void)
{
// MPC5777C - FEC MII-Lite mode IO setting
SIU.PCR[99].R = PA_ALT2 | OBE | IBE | SRC | WPE; // FEC_MDIO
SIU.PCR[109].R = PA_ALT3 | OBE | WPE; // FEC_MDC
SIU.PCR[252].R = PA_PRIM | ODE | SRC; // FEC_TX_EN
SIU.PCR[248].R = PA_PRIM | ODE | SRC; // FEC_TXD0
SIU.PCR[251].R = PA_PRIM | ODE | SRC; // FEC_TXD1
SIU.PCR[98].R = PA_ALT2 | ODE | SRC; // FEC_TXD2
SIU.PCR[101].R = PA_ALT3 | ODE | SRC; // FEC_TXD3
SIU.PCR[474].R = PA_PRIM | IBE | WPE; // FEC_TX_CLK
SIU.PCR[100].R = PA_ALT3 | IBE | SRC | WPE; // FEC_RX_CLK
SIU.PCR[249].R = PA_PRIM | IBE | WPE; // FEC_RX_DV
SIU.PCR[250].R = PA_PRIM | IBE | SRC | WPE; // FEC_RXD0
SIU.PCR[253].R = PA_PRIM | IBE | SRC | WPE; // FEC_RXD1
SIU.PCR[110].R = PA_ALT3 | IBE | SRC | WPE; // FEC_RXD2
SIU.PCR[107].R = PA_ALT3 | IBE | SRC | WPE; // FEC_RXD3
}
2. FEC Clock setting
- According to 'MPC5777C_EVB_USER_GUIDE' document, on Board FEC 50MHz CLK is enable with J524 jumper setting.
- With that jumper setting, if I set the 'MII Speed Control Register(FEC_MSCR)' with '0xA', it results in an 'FEC_MDC frequency 2.5MHz. Is that right?
3. isConnected() function
- It's kind of stuck in 'while (!isConnected())'
- In my case, the miiRead return data is always '0x7849', so the 'result = (data & 0x0004) ? 1 : 0' is always '0'.
- What is the meaning of register address value of '0x0001' in isConnected() function?
- How can I pass and return expected data from miiRead() function? Please guide me.
// isConnected - returns 1 is connected, otherwise 0
int isConnected(void)
{
uint16_t data;
int result = 0;
if (miiRead(0x0001, &data))
{
result = (data & 0x0004) ? 1 : 0;
}
return result;
}
int miiRead(int regAddr, uint16_t *data)
{
...
FEC.MMFR.R = 0x60020000 | ((phyAddr & 0x1F) << 23) | ((regAddr & 0x1F) << 18);
}
I couldn't upload full source code for the security reasons, please refer 'AN4577SW' sample code.
If there are any advice, feedback or sample code, please let me know.
Thank you for your patience.
Hi.
I used the same configuration described in the last post. But it is not working.
Using wireshark the ARP packets generated by the processor is not received on the HOST.
The processor is receiving some packets sent by the HOST but with wrongly size and type.
I am using a MPC57xx MB Rev C,
The Jumper Configuration
J24 is 1-2.
J510 is 1-2.
J514 is 2-3.
The function isConnected is return TRUE when the cable is Connected.
Is it possible with a wrong clock configuration ?
I used the same clock configuration as the example Example_MPC5777C-PinToggleStationery.
Thanks
Hi,
Note: on Rev.A of the EVB minimodules the RXD2 and RXD3 are not directly connected to the PHY. Also there is no 50MHZ oscillator, which is needed for RMII mode. This is fixed on mini-modules of rev.B or higher.
BR, Petr
Thank you for the reply.
I forgot to mention that the EVB is rev.C.
I have corrected the I/O setting and the clock setting.
1. There were some mistakes of I/O setting. It supposed to be OBE, not ODE.
- Also I added SIU_IMUX0 register setting for input pins, please check if I set it correctly.
// initFecIo - initialise pads for FEC use in the SIU
void initFecIo(void)
{
// MPC5777C - FEC MII-Lite mode IO setting
SIU.PCR[PCR99_FEC_MDIO_ALT2].R = PA_ALT2 | OBE | IBE | SRC | WPE; //FEC_MDIO
SIU.PCR[PCR109_FEC_MDC_ALT3].R = PA_ALT3 | OBE | WPE; //FEC_MDC
SIU.PCR[PCR252_FEC_TX_EN_PRIM].R = PA_PRIM | OBE | SRC; //FEC_TX_EN
SIU.PCR[PCR248_FEC_TXD0_PRIM].R = PA_PRIM | OBE | SRC; //FEC_TXD0
SIU.PCR[PCR251_FEC_TXD1_PRIM].R = PA_PRIM | OBE | SRC; //FEC_TXD1
SIU.PCR[PCR98_FEC_TXD2_ALT2].R = PA_ALT2 | OBE | SRC; //FEC_TXD2
SIU.PCR[PCR101_FEC_TXD3_ALT3].R = PA_ALT3 | OBE | SRC; //FEC_TXD3
SIU.PCR[PCR474_FEC_TX_CLK_PRIM].R = PA_PRIM | IBE | WPE; //FEC_TX_CLK
SIU.PCR[PCR100_FEC_RX_CLK_ALT3].R = PA_ALT3 | IBE | SRC | WPE; //FEC_RX_CLK
SIU.PCR[PCR249_FEC_RX_DV_PRIM].R = PA_PRIM | IBE | WPE; //FEC_RX_DV
SIU.PCR[PCR250_FEC_RXD0_PRIM].R = PA_PRIM | IBE | SRC | WPE; //FEC_RXD0
SIU.PCR[PCR253_FEC_RXD1_PRIM].R = PA_PRIM | IBE | SRC | WPE; //FEC_RXD1
SIU.PCR[PCR101_FEC_RXD2_ALT3].R = PA_ALT3 | IBE | SRC | WPE; //FEC_RXD2
SIU.PCR[PCR107_FEC_RXD3_ALT3].R = PA_ALT3 | IBE | SRC | WPE; //FEC_RXD3
//Input Multiplexing Register0(SIU_IMUX0) setting for FEC input pins
SIU.IMUX0.R = IMUX0_MUXSEL6_FEC_TXCLK | IMUX0_MUXSEL1_FEC_RXDV | IMUX0_MUXSEL2_FEC_RXD0 | \
IMUX0_MUXSEL5_FEC_RXD1 | IMUX0_MUXSEL11_FEC_RXD2 | IMUX0_MUXSEL8_FEC_RXD3;
}
2. Could you explain more details about FEC clock setting? (MII-Lite interface)
- I couldn't find any guideline to set FEC clock. Can you list up what register are needed to set and how they work?
- Please check 'peripheral clock setting' below
#define SIU_SYSDIV_PERCLKSEL_NON_FM_CLOCK 0x1000000
#define SIU_SYSDIV_PERDIV_DIVIDE_BY_2 0x0000000
...
//Peripheral Clock Setting, 50MHz / 2 => 25 MHz(Internal bus clock)
SIU.SYSDIV.R = SIU_SYSDIV_PERCLKSEL_NON_FM_CLOCK | SIU_SYSDIV_PERDIV_DIVIDE_BY_2;
...
FEC.MSCR.B.MII_SPEED = 0x5; // 25MHz x (1 / ( 5 x 2 )) = 2.5MHz
Thank you.