Question about SPI_1 module can not output signal at PIN PA[6](clock) and PA[7](MOSI) in S32R274

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about SPI_1 module can not output signal at PIN PA[6](clock) and PA[7](MOSI) in S32R274

Jump to solution
2,648 Views
nxf49919
NXP Employee
NXP Employee

Hi

The S32R274 has two SPI devices: SPI_1 and SPI_2, and there is no difference in the RM description.

I found that using the same SPI and pin(SIUL2) register configuration, other pins can output clock and data signals, but PA [6] and PA [7] cannot output signals, as shown in the following table:

 

PIN

Module

function

Register value

OUTPUT

PA[6]

SPI_1

SCK

0x12840001

Without output signal

PB[2]

0x12840004

Output clock signal

PA[7]

MOSI

0x12840001

Without output signal

PA[9]

0x12840004

Output data signal

PA[0]

SPI_2

SCK

0x12840002

Output clock signal

PA[11]

0x12840001

Output clock signal

PA[1]

MOSI

0x12840002

Output data signal

PA[12]

0x12840001

Output data signal

SPI_1 supports the following pins:

  CLK:   PA [6], PB [2]

  MOSI: PA [7], PA [9]

  MISO: PA [8], PB [3], PH [7]

SPI_2 supports the following pins:

  CLK:   PA [0], PA [11]

  MOSI: PA [1], PA [12]

  MISO: PA [2], PA [13]

Chip selections pins and data input pins are not listed.

When use any SPI_2 configuration or SPI_1 use PB[2] as clock and PA[9] as output, the signal is normal, but PA[7] and PA[6] cannot output signal under the same configuration.

I used the correct pin register MSCR and SPI register configuration according to the reference manual, and I saw the register write the correct value in debug mode in real time.

Thanks!

1 Solution
2,492 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I did quick test on EVB and it works as expected, I can see nice signals on my scope. My test code is attached (copied from other projects, maybe some comments are not valid).

If you use EVB, PA6 and PA7 are available on J13 on the adapter:

pastedImage_1.png

Regards,

Lukas

View solution in original post

0 Kudos
Reply
7 Replies
2,493 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I did quick test on EVB and it works as expected, I can see nice signals on my scope. My test code is attached (copied from other projects, maybe some comments are not valid).

If you use EVB, PA6 and PA7 are available on J13 on the adapter:

pastedImage_1.png

Regards,

Lukas

0 Kudos
Reply
2,492 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

pastedImage_1.png

2,492 Views
nxf49919
NXP Employee
NXP Employee

Hi Lukas

Thank you very much, your test is right.

When I test again, I also observed the output signal in PA[6] and PA[7] by J13.

I already know the reason.

Only PA[8] PA[7] PA[6] in the MPC57XXXMB Evaluation Board Motherboard which I use to test did not connet to S32R274 corresponding pad.

So I only can observe the PA[6] PA[7] PA[8] output signal in Daughterboard J13.

We can output SPI_1 signal in PA7[channel1], PA9[channel2], PA6[channel3] signal as follow:

波形.PNG

Best Regards

Huaqiang

0 Kudos
Reply
2,492 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Huaqiang,

it's mentioned in the user guide, section 5. Board interface connector:

https://www.nxp.com/docs/en/user-guide/S32R274-EVBUG.pdf 

pastedImage_2.png

Regards,

Lukas

0 Kudos
Reply
2,492 Views
nxf49919
NXP Employee
NXP Employee

Hi Lukas

Thank you I undrstand.

section 5. Board interface Connector is very useful for test signal.
Best Regards

Huaqiang

0 Kudos
Reply
2,492 Views
nxf49919
NXP Employee
NXP Employee

Hi David

This is the value of MSCR[n] register in S32R274 SIUL2 module, details as follow:

PIN

Module

function

Register

value

OUTPUT

PA[6]

SPI_1

SCK

SUIL2.MSCR[6]

0x12840001

Without output signal

PB[2]

SUIL2.MSCR[18]

0x12840004

Output clock signal

PA[7]

MOSI

SUIL2.MSCR[7]

0x12840001

Without output signal

PA[9]

SUIL2.MSCR[9]

0x12840004

Output data signal

PA[0]

SPI_2

SCK

SUIL2.MSCR[0]

0x12840002

Output clock signal

PA[11]

SUIL2.MSCR[11]

0x12840001

Output clock signal

PA[1]

MOSI

SUIL2.MSCR[1]

0x12840002

Output data signal

PA[12]

SUIL2.MSCR[12]

0x12840001

Output data signal

Thank you

0 Kudos
Reply
2,492 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, which register the table above points to?

0 Kudos
Reply