Question about MPC5748G MCU variants

cancel
Showing results for 
Search instead for 
Did you mean: 

Question about MPC5748G MCU variants

195 Views
jch050226
Contributor II

Hello!

I have a question about the name's meaning of MPC5748g MCU.

in MCU's name, there is Optional fields.

if this has S it means HSM(Security Module).

if my MPC5748g is HSM, is it impossible to use CAN FD?

full name is SPC5748GSMKU6 1N81M QAD1731AD

thanks

Sincerely yours.

pastedImage_1.png

2 Replies

132 Views
jch050226
Contributor II

Thank you so much! :smileyhappy:

0 Kudos

132 Views
petervlna
NXP Employee
NXP Employee

Hello,

if my MPC5748g is HSM, is it impossible to use CAN FD?

full name is SPC5748GSMKU6 1N81M QAD1731AD

No.

As the table say it is required to have at least B version or H to be able to use both HSM and CANFD.

Furthermore S means that there is only HW HSM module with no FW from NXP. You have to write it on your own if you wan to use the HSM module.

regards,

Peter