Progppcnexus can not connect MPC5748G-LCEVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Progppcnexus can not connect MPC5748G-LCEVB

1,509 Views
mgdsun2000
Contributor I

The mpc5748g-lcevb development board I purchased is powered on after connecting to progppcnexus. After clicking connect, the following interface appears. The target may have entered reset escalation. Please power cycle the board.

Power on repeatedly according to the following prompts, and the phenomenon is still.

What is the problem? How to solve it?

1111.png

0 Kudos
Reply
2 Replies

1,491 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

The reason will be probably due to feature newly introduced with MPC57xx devices - it is called 'Functional' Reset Escalation and 'Destructive' Reset Escalation (MC_RGM_FRET and MC_RGM_DRET) and it causes that after predefined number of functional reset, destructive reset happen and after predefined number of destructive resets, device will stay in reset until next POR.

The solution is to stop the core just after power-on-reset, attach by debugger and erase MCU/reload the code.
With TRACE32 it can be done by “Halt core at power-on reset” feature (Select in the menu: MPC5XXX - Tools - Halt core at power-on reset.).

If you have only PeMicro debugger available, I have found another thread describing how to attach with PeMicro:
https://community.nxp.com/thread/504643

Also check whether you have properly attached power to the board (DEVKITs and similar boards may have jumpers for selecting power from USB or 5V barrel connector) and sometimes you may see such warning when MCU is just unpowered because of 5V power supply is not attached.

0 Kudos
Reply

1,460 Views
mgdsun2000
Contributor I

Connection from "127.0.0.1" via 127.0.0.1

PE-ERROR: Warning. Can't read registers while part is running. Copyright 2012 P&E Microcomputer Systems,Inc.

Command Line :C:\NXP\S32DS_Power_v1.2\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.6.9.201706282002\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=1000 -port?

CMD>RE

Initializing.

Cannot enter background mode.

Check connections.

Error Resetting device for programming.

Starting reset script (C:\NXP\S32DS_Power_v1.2\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.6.9.201706282002\win32\gdi\P&E\s32e200_mpc574xg.mac) ...

REM This script is compatible with MPC574xG devices.

REM Clean GPRs to remove residual data after using algorithm

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

Error : Error in ONCE status register during instruction execution.

REM Initialize all of the Main SRAM - 768KB

Initializing RAM from $40000000 to $400BFFFF.

REM Core 0 I-MEM 16K

Initializing RAM from $50000000 to $50003FFF.

REM Core 0 D-MEM 64K

Initializing RAM from $50800000 to $5080FFFF.

REM Core 1 I-MEM 16K

Initializing RAM from $51000000 to $51003FFF.

REM Core 1 D-MEM 64K

Initializing RAM from $51800000 to $5180FFFF.

REM Core 2 I-MEM 16K

Initializing RAM from $52000000 to $52003FFF.

REM Core 2 D-MEM 32K

Initializing RAM from $52800000 to $52807FFF.

REM overlay memory 16K

Initializing RAM from $0D000000 to $0D003FFF.

REM Overlay SRAM Emulation device only Initializing RAM from $0C000000 to $0C0FFFFF.

Reset script (C:\NXP\S32DS_Power_v1.2\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.6.9.201706282002\win32\gdi\P&E\s32e200_mpc574xg.mac) completed.

MPC574xG Device detected.

PE-ERROR: Error downloading to the device.

Disconnected from "127.0.0.1" via 127.0.0.1

Target Disconnected.

Target Disconnected.

0 Kudos
Reply