Power Consumption Reduction on MPC5673F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Power Consumption Reduction on MPC5673F

423 次查看
jaskaranjeetsin
Contributor I

Hi, I am looking for a solution to reduce the power consumption of the mcu MPC5673F. The Issue is that during a power fail we should be able to save certain number of bytes in the Flash, before the energy buffer is depleted. With the current Hardware, it is not possible to save 128 bytes in the Flash. Increasing Size of the capacitor (energy buffer) is not possible.

 

Can someone provide a solution for this Problem?

标签 (1)
0 项奖励
1 回复

336 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if you can't change the hardware, you can:

- re-configure output pins, so external load is minimized.

- use SIU_HLT register to stop peripherals.

- decrease the system clock. Erase/program operation is self-clocked, it does not depend on system clock.

Regards,

Lukas

0 项奖励