we have a chip of 5744 with hardware problem "TMS pin shorted to GND", and we have done the further analysis with the help of NXP. the further analysis report identified the damage region like below.
we want to know these damage region will how effect on behavior of 5744.
Hi,
I don't know the background of your question but if the TMS pin does not work, you won't be able to use JTAG for debug. If only the TMS pad structure is damaged in a way that no further damage can occur (domino effect), it should not affect the rest of the chip.
Regards,
Lukas
Thanks for your response. we do not be able to use JTAG for debug. but we also have other strange problem about software. See below:
1. the chip can not run when its temperature is low, but working when its temperature becoming high.
2. software run over without any code error.
we want to know the reason about problem like above, but we have nothing way to test it. and now we only know the TMS pin was damaged.
so we want some suggestion about how to assess this damage point bring to 5744 chip and the possible relevance with the software problems.
I'm afraid that there's no way to find out the root cause without JTAG interface.
Can you see this behavior only on this one chip which has damaged TMS pin? Are other boards working as expected?
Regards,
Lukas
we only see this behavior on two chips which has damaged TMS pin. there are not this behavior on chips without damaged TMS pin.
It seems this is something I cannot help with. It's impossible to debug the chip without JTAG.
Regards,
Lukas