PLL reconfiguration on MPC5744P

cancel
Showing results for 
Search instead for 
Did you mean: 

PLL reconfiguration on MPC5744P

508 Views
qm1013
Contributor III

hello, I have got a problem, when use  the MPC5744P .

Here is the problem:

In the Flash Boot Loader the PLL is configured , when the app is flashed, the MCU will reset, and jump to app, in the app the PLL still need to be configured, then the problem happened, the MCU was dead. I think it may be the PLL reconfiguration problem. 

Will you have some suggestions on PLL reconfiguration ? 

I am looking forward to the suggestions.

regards,

meng

Tags (3)
0 Kudos
1 Reply

432 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

then the problem happened, the MCU was dead

What should we imagine under this issue description?

What is the content of RGm{FES/DES] registers? Did Watchdog react?

Where the code is stuck?

Is it possible to connect to device with debugger after the issue?

regards,
Peter

0 Kudos