PIT & RTI Load Values in MPC5644A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PIT & RTI Load Values in MPC5644A

1,745 次查看
turgay_kale
Contributor III

Hi,

I have been facing wrong PIT and RTI load register values in MPC5644A microcontroller. My board has a crystal oscillator that drives at 40 MHz and microcontroller system frequency is at 150 MHz. I want to use RTI timer for generating an interrupt for every 1 ms and want to use PIT0 for measuring the time triggered from RTI timer.

freq_rti = 40 MHz thus period for a single RTI pulse is 1 / 40.000.000 = 25 ns

freq_pit0 = 150 MHz thus period for a single PIT pulse is 1 / 150.000.000 = 6,667 ns

***************************************************************************************************************

#define RTI_READ_LOAD_VALUE             PIT.RTI.CVAL.R

#define RTI_INTERRUPT_FLAG                 PIT.RTI.TFLG.R

#define PIT0_READ_LOAD_VALUE           PIT.TIMER[0].CVAL.R 

static void RTI_init (void)
{
   PIT.PITMCR.B.MDIS_RTI = 0;     // clear MDIS_RTI; enable clock for RTI
   PIT.PITMCR.B.FRZ = 1;              // Timers are stopped in debug mode
   PIT.RTI.LDVAL.R = 40.000.000 / 1000 - 1;     // RTI load register value for generating interrupt for every 1 ms
   PIT.RTI.TCTRL.B.TIE = 1;                              // let RTI generate interrupts
   PIT.RTI.TCTRL.B.TEN = 1;                            // start RTI

   // assign interrupt function for RTI ISR vector number
   INTC_InstallINTCInterruptHandler(doSlotBasedTaskScheduling, 305, 1);       // RTI vector: 305
}

static void PIT0_init (void)

{

   /* 30: MDIS = 0 to enable clock for PITs. */
   /* 31: FRZ = 1 for Timers stopped in debug mode */
   PIT.PITMCR.R = 0x00000001;
   PIT.TIMER[0].LDVAL.R = (150.000.000 / 1000) * 10 - 1; // PIT0 load value to measure 10 ms time range

   /* clear the TIF flag */
   PIT.TIMER[0].TFLG.R = 0x00000001;

   /* 30: TIE = 0 for interrupt request disabled */
   /* 31: TEN = 1 for timer active */
   PIT.TIMER[0].TCTRL.R = 0x00000001;

}

GLOBAL void doSlotBasedTaskScheduling (void)
{
   /* This function will be called for every 1 ms from the INTC module */

  RTI_INTERRUPT_FLAG = 0x00000001;     // clear RTI timer interrupt flag

   if (counterX < 2000)
   {
      array_period_rti[counterX] = RTI_READ_LOAD_VALUE;
      array_period_pit0[counterX] = PIT0_READ_LOAD_VALUE;

      counterX++;
   }

}

***************************************************************************************************************

P.M. RTI timer is sourced from the external crystal oscilator thus there may be a bunch of delayed cycles for reading RTI values.

I expect to read approximately 40.000 - 1 - delay_rti = ~39.999 cycles (1 ms) from the RTI load register value but I read 3977. And I couldn't understand why.

pastedImage_7.png

And similarly, I expect to read approximately 150.000 - 1 = ~ 149.999 cycles (1 ms) between two ordered PIT0 load register value readings but I read approximately 15.000 cycles (ex.119.966-104.976 = ~14.990) between two ordered PIT0 readings. 

pastedImage_2.png

Would you pls help me to fix the problem?

Thank you.

标签 (1)
0 项奖励
6 回复数

1,603 次查看
turgay_kale
Contributor III

Petr hi,

Thank you for your suggestions, I couldn't check the time by scope yet but with the debugger I checked the CVAL and LDVAL values are changing as you can see below, values jump from ~4.000 to ~40.000 level at 782. call of doSlotBasedTaskScheduling() function. Do you have a forecast for that effect?

pastedImage_2.png

#define TASK_TIMER_NEW_LOAD_VALUE              PIT.RTI.LDVAL.R
#define TASK_TIMER_CURRENT_LOAD_VALUE       PIT.RTI.CVAL.R

GLOBAL void doSlotBasedTaskScheduling(void)
{
   /* This function will be called for every 1 ms from the INTC module */

   TASK_TIMER_INTERRUPT_FLAG = 0x00000001;


   if (counterX < 2000)
   {
      array_period_rti_ldval[counterX] = TASK_TIMER_NEW_LOAD_VALUE;
      array_period_rti_cval[counterX] = TASK_TIMER_CURRENT_LOAD_VALUE;

      counterX++;
   }

}

Regards,

0 项奖励

1,603 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

it looks the LDVAL is changed during runtime. Could this be the case in your code?

BR, Petr

0 项奖励

1,602 次查看
turgay_kale
Contributor III

Hi Petr,

LDVAL is only set in the initialization function as PIT.RTI.LDVAL.R = 39.999.

Regards,

0 项奖励

1,603 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if a debugger has an option to put breakpoint on register write, use it for LDVAL.

BR, Petr

0 项奖励

1,603 次查看
turgay_kale
Contributor III

Dear Petr,

I determined to use PIT instead of RTI timer. Therefore you can close the issue. Thank you very much for your help and support.

Regards,

0 项奖励

1,603 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

try to check RTI.CVAL and RTI.LDVAL values within debugger and also measure generated interval by scope (toggle some pin). Do you see expected results?

BR, Petr

0 项奖励