Hello,
I am developing Ethernet communication using MPC5775B.
ENET and PHY modules are incorporated. PHY used is KSZ8061RNB and the PHY type chosen is Phy Generic.
RMII Mode is chosen. Auto negotiation and AutoMDIx configurations are enabled.
Pin strapping Config: 111 (RMII Normal Mode and AutoMDIx)
During run time, I verified all the FEC registers and PHY registers.
I could find the FEC_EIMR, ECR, MSCR, MMFR, TCR and RCR Register values proper, and all intended configurations are reflected in the internal registers,
except that the PHY_Read is always returning 0xFFFF.
Steps taken to troubleshoot:
The power supply is stable. VDDIO and RefClk are stable. No FEC Error flags are set.
1. Checked if the system is stuck in reset state. ECR register is telling that the reset is asserted, acknowledged and deasserted successfully on FEC.
Probed on Reset pin of PHY and confirmed that it's released and stable before read attempt.
2. Checked the Phy Address configuration. It is configured to be 0x01 via HW Pin strapping and also in Software. This is getting reflected in MMFR Register.
3. A pull down is given on RXD0 for enabling auto negotiation.
4. Checked the pull up on MDIO line (1K pullup).
5. Tried reducing the MDC frequency from 2.5MHz to 1MHz.
6. Probed on MDC line and confirmed that the clock is stable.
7. Checked the MII Field of MSCR Register and the MII speed is proper (49d or 31h with FEC0_Clk as 100MHz, when MDC frequency is 1MHz) (19d or 13h with FEC0_Clk as 100MHz, when MDC frequency is 2.5MHz).
8. Scanned all Phy addresses (0x00 to 0x1F). All are returning 0xFFFF.
9. Probed on MDIO line and checked the activity while read and write operation, keeping a GPIO as trigger.
10. The MDIO activity is verified via serial monitor logs.
Observation:
Please find the FEC Register values below.
FEC Error Flags: 0x00000000
EIMR Register: 0x6A780000
MSCR Register: 0x00000026
MMFR Register: 0x6083FFFF
ECR Register: 0xF0000002
TCR Register: 0x00000004
RCR Register: 0x05EE012C
The opmode, start frame delimiter, register address and phy address fields of MMFR are proper.
However, there is no low pulse on MDIO in the Turn Around + Data phase.
That means PHY is not acknowledging MDIO read.
As per my understanding, the FEC module handles the turnaround and data driving portions of MDIO reads internally.
I have attached the Observation on CRO, herewith.
Please check and let me know what change is required to get the PHY respond with proper TA and Data phase.


Thanks, and Kind Regards,
Divya