PEC mode in EMIOS MPC5777c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PEC mode in EMIOS MPC5777c

Jump to solution
1,087 Views
dineshmoka
Contributor III

hi i am using the MPC5777c EMIOS module in PEC mode for counting the number of pulses given to input channel. The following below is my code

void D_EMIOS_0_PEC_Init(uint8_t ui8_channel_no,uint16_t ui16_GPIO_pin_no)
{
SIU.PCR[ui16_GPIO_pin_no].R = 0x0500;
eMIOS_0.MCR.B.GPRE = 0x81;   //130/129+1 = 1MHz
eMIOS_0_UC.UC[ui8_channel_no].A.R = 0;
eMIOS_0_UC.UC[ui8_channel_no].B.R = 10;
eMIOS_0_UC.UC[ui8_channel_no].C.B.EDPOL = 1;
eMIOS_0_UC.UC[ui8_channel_no].C.B.MODE = 0x1;

eMIOS_0.MCR.B.GPREN = 0;
eMIOS_0.MCR.B.FRZ = 1;

eMIOS_0_UC.UC[ui8_channel_no].C.B.UCPREN = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.FREN = 1;
eMIOS_0_UC.UC[ui8_channel_no].CNT.R = 0x0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.BSL = 0x3;
eMIOS_0_UC.UC[ui8_channel_no].C.B.ODIS = 1;
eMIOS_0_UC.UC[ui8_channel_no].C.B.FCK = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.IF = 0x0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.FCK = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.MODE = 0x0B;
eMIOS_0_UC.UC[ui8_channel_no].A.R = 0;
eMIOS_0_UC.UC[ui8_channel_no].B.R = 10;
eMIOS_0_UC.UC[ui8_channel_no].C.B.UCPRE = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.EDPOL = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.EDSEL = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.UCPREN = 1;

eMIOS_0.MCR.B.GPREN = 1;
eMIOS_0.MCR.B.GTBE = 1;
}

by using function generator i gave 1MHz pulses to the input channel i.e. CH[2] GPIO[181]. Can you please check any error is there in my code ,i am not getting any output value my both registers EMIOS_CNTn register and EMIOS_ALTAn registers are showing zero only.

 

0 Kudos
1 Solution
1,071 Views
dineshmoka
Contributor III

hi petrs

Can i get the example code for configuring IGF module

View solution in original post

0 Kudos
5 Replies
1,072 Views
dineshmoka
Contributor III

hi petrs

Can i get the example code for configuring IGF module

0 Kudos
1,060 Views
PetrS
NXP TechSupport
NXP TechSupport
0 Kudos
1,049 Views
dineshmoka
Contributor III

hi petrs, based on that example i modified my code still am not getting my output.Following below is my code 

void D_EMIOS_0_PEC_Init(uint8_t ui8_channel_no,uint16_t ui16_GPIO_pin_no)
{
SIU.PCR[ui16_GPIO_pin_no].R = 0x0500;
eMIOS_0.MCR.B.GPRE = 0x81;
eMIOS_0_UC.UC[ui8_channel_no].A.R = 0;
eMIOS_0_UC.UC[ui8_channel_no].B.R = 10;
eMIOS_0_UC.UC[ui8_channel_no].C.B.EDPOL = 1;
eMIOS_0_UC.UC[ui8_channel_no].C.B.MODE = 0x1;

// set IGF to filter low pulses <1.5us
IGF_0.FTHR.B.FTH = 0x82; // falling threshold = pulse width * clock = 1us*130Mhz = 130
IGF_0.MCR18.B.RFM = 0x0; // rising edge: bypassed
IGF_0.MCR18.B.FFM = 0x2; // falling edge: integrated type
IGF_0.MCR18.B.FGEN = 0x1; // enable filter

eMIOS_0.MCR.B.GPREN = 0;
eMIOS_0.MCR.B.FRZ = 1;

eMIOS_0_UC.UC[ui8_channel_no].C.B.UCPREN = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.FREN = 1;
eMIOS_0_UC.UC[ui8_channel_no].CNT.R = 0x0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.BSL = 0x0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.ODIS = 1;
eMIOS_0_UC.UC[ui8_channel_no].C.B.FCK = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.IF = 0x0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.FCK = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.MODE = 0x0B;
eMIOS_0_UC.UC[ui8_channel_no].A.R = 0;
eMIOS_0_UC.UC[ui8_channel_no].B.R = 10;
eMIOS_0_UC.UC[ui8_channel_no].C.B.UCPRE = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.EDPOL = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.EDSEL = 0;
eMIOS_0_UC.UC[ui8_channel_no].C.B.UCPREN = 1;

eMIOS_0.MCR.B.GPREN = 1;
eMIOS_0.MCR.B.GTBE = 1;
}

0 Kudos
1,000 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

what if you only enable IGF in bypassed mode, so use only IGF_0.MCR18.B.FGEN = 0x1; // enable filter and comment other IGF setting.

Also A1 holds the start time and B1 holds the stop time for the time window. You selected counter bus A as timebase, so do you have CH23 configured and running, thus a match with A1 can clear PEC internal counter and start counting external events?

BR, Petr

0 Kudos
1,080 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you will need to configure IGF module, otherwise inputs does not pass to eMIOS module. For eMIOS_0 ch2 it should be IGF_0 ch18

IGF_0.FILTER[18].MCR.B.FGEN = 1;

 

BR, Petr

 
0 Kudos