P&E Mirco (gdb) debug error " No source available: 0x10" with MPC5744p + Diab compiler + S32D IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P&E Mirco (gdb) debug error " No source available: 0x10" with MPC5744p + Diab compiler + S32D IDE

1,495 Views
yaohe
Contributor I

Development Environment:

MCU: MPC5744P

Compiler + Linker : WindRiver Diab Compiler v5.9.4.0 (dcc + dld)

IDE: S32 Design Studio  for PowerPC V1.0

Debugger: P&E USB multilink (GDB server)

 

I creat a test project, build with no errors, but while I download the code to the MCU and begin debug, the debugger display error: No source available : 0x10, the MCU even not run to the _start.

Original Attachment has been moved to: Diab_mpc5744_test_vle.rar

Labels (1)
0 Kudos
Reply
1 Reply

1,287 Views
yaohe
Contributor I

Hi, everybody, can someone share a test program (mpc5744p+diab compiler+S32 Design Studio+P&E mirco Debugger )with me? I have try construct this development environment long time, but always have some problems. Thank you very much!

0 Kudos
Reply