Not all FlexCAN working MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not all FlexCAN working MPC5748G

790 Views
xenon77
Contributor I

Hi,

I´m using the DEVKIT-MPC5748G and DEVKIT-COMM to develop a CAN gateway. I need to use 5 FlexCANs. Everything is working with FlexCAN_0, 1 and 3 but FlexCAN_5 and 7 will not work. Forced to used those FlexCANs due to they are available on the DEVKITs. Project compiles and uploads ok to the board but when I´m trying to send messages to the board I get error frames on FlexCAN_5 and 7, but FlexCAN_0, 1 and 3 is ok. This is my code:

FlexCAN_0 that is working

/********************************************************************************/
/* Initialize FlexCAN_0 GWCAN0 */

/********************************************************************************/

void FlexCAN_0_init(void)

{

/* Int used in for-loops */

int i = 0;

/* Set IRQ for FlexCAN_0 RX */

//INTC.PSR[568].R = 0xF; //set interrupt core and priority

/* Configure GPIO for FlexCAN_0 */

SIUL2.MSCR[16].B.SSS = 1; /* Pad PB0: Source signal is CAN0_TX */

SIUL2.MSCR[16].B.OBE = 1; /* Pad PB0: Output Buffer Enable */

SIUL2.MSCR[16].B.SRC = 3; /* Pad PB0: Maximum slew rate */

SIUL2.MSCR[17].B.IBE = 1; /* Pad PB1: Enable pad for input - CAN0_RXD */

SIUL2.IMCR[188].B.SSS = 2; // CAN0_RX: connected to pad PB1 ** FUNKAR!! ***

/* Configure FlexCAN_0 module */

CAN_0.MCR.B.MDIS = 1; // Disable module before selecting clock source

CAN_0.CTRL1.B.CLKSRC = 0; // Clock source is oscillator clock (40MHz)

CAN_0.MCR.B.MDIS = 0; // Enable module for configuration (Sets FRZ, HALT)

while (!CAN_0.MCR.B.FRZACK) {} // Wait for freeze acknowledge to set

CAN_0.CTRL1.R = SetCTRL1(); // CAN bit timing

CAN_0.RXFGMASK.R = 0; // Global acceptance mask FIFO 0 = Accept all

/* Clear all RX individual Mask Registers */

for(i = 0; i < 96; i++) { CAN_0.RXIMR[i].R = 0; }

CAN_0.IFLAG1.R = 0xFFFFFFFF; // Clear all RX flags

/* Leave freeze mode and start module with 32 MBs */

CAN_0.MCR.R = SetMCR(); // Enable module with settings

while (CAN_0.MCR.B.FRZACK & CAN_0.MCR.B.NOTRDY) {} /* Wait to clear */

}

FlexCAN_5 that is not working

/********************************************************************************/

/* Initialize FlexCAN_5 GWCAN5 */

/********************************************************************************/

void FlexCAN_5_init(void)

{

/* Int used in for-loops */

int i = 0;

/* Set IRQ for FlexCAN_5 RX */

//INTC.PSR[628].R = 0xF; //set interrupt core and priority

/* Configure GPIO for FlexCAN_5 */

SIUL2.MSCR[65].B.SSS = 1; /* Pad PE1: Source signal is CAN5_TX */

SIUL2.MSCR[65].B.OBE = 1; /* Pad PE1: Output Buffer Enable */

SIUL2.MSCR[65].B.SRC = 3; /* Pad PE1: Maximum slew rate */

SIUL2.MSCR[64].B.IBE = 1; /* Pad PE0: Enable pad for input - CAN5_RXD */

SIUL2.IMCR[193].B.SSS = 1; /* CAN5_RX: connected to pad PE0 */

/* Configure FlexCAN_5 module */

CAN_5.MCR.B.MDIS = 1; // Disable module before selecting clock source

CAN_5.CTRL1.B.CLKSRC = 0; // Clock source is oscillator clock (40MHz)

CAN_5.MCR.B.MDIS = 0; // Enable module for configuration (Sets FRZ, HALT)

while (!CAN_5.MCR.B.FRZACK) {} // Wait for freeze acknowledge to set

CAN_5.CTRL1.R = SetCTRL1(); // CAN bit timing

CAN_5.RXFGMASK.R = 0; // Global acceptance mask FIFO 0 = Accept all

/* Clear all RX individual Mask Registers */

for(i = 0; i < 96; i++) { CAN_5.RXIMR[i].R = 0; }

CAN_5.IFLAG1.R = 0xFFFFFFFF; // Clear all RX flags

/* Leave freeze mode and start module with 32 MBs */

CAN_5.MCR.R = SetMCR(); // Enable module with settings

while (CAN_5.MCR.B.FRZACK & CAN_5.MCR.B.NOTRDY) {} /* Wait to clear */

}

Return of SetCTRL1(); is 0x09DB0086 

250 kbps

Return of SetMCR(); is 0x2002000C

FIFO enabled, SRXDIS enabled, 12 mailboxes

As you can see the settings are the same. I have checked and double checked the SIUL2 settings and aslo consluted the RM attached XLS sheet to see that the IMCR SSS is correct.

DEVKIT-MPC5748G is rev B and DEVKIT-COMM is rev A.

I´m using S32DS for Power Architecture 2017.R1 build 171018

Thankfull for help!

Best regards, Joakim

Tags (3)
0 Kudos
Reply
0 Replies