Not able to launch debug trace with JTAG on Z2 on MPC5748 EVB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to launch debug trace with JTAG on Z2 on MPC5748 EVB

Jump to solution
879 Views
karma_JC
Contributor I

Hi:

Is there anyway to launch debug trace on individual core in MPC5748?  I have set up Z2 with SDK.  I try to launch debug trace. However, after some wait, the following message comes out :

Error in final launch sequence
Failed to execute MI command:
-target-select remote localhost:7228
Error message from debugger back end:
localhost:7228: The system tried to join a drive to a directory on a joined drive.
localhost:7228: The system tried to join a drive to a directory on a joined drive.

Is there a way to debug and trace program from individual core, and how????

Thank you

James

0 Kudos
Reply
1 Solution
855 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

expected use case is either to launch debug session for single boot core only or to launch debug session for all cores using "Launch Group" debug configuration.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
2 Replies
856 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

expected use case is either to launch debug session for single boot core only or to launch debug session for all cores using "Launch Group" debug configuration.

Regards,

Lukas

0 Kudos
Reply
843 Views
karma_JC
Contributor I

Hi Lukas:

I found some examples of multi-core. I realized that "debug" can only launch on boot core.

Thanks

James

0 Kudos
Reply