No source available for "SWT1_IRQHandler() at 0x811800"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No source available for "SWT1_IRQHandler() at 0x811800"

Jump to solution
990 Views
berat24
Contributor III

Hello everyone,

I configured SWT to move to interrupt on first time-out and then reset on second time-out. However, I am taking the fault, No source available for "SWT1_IRQHandler() at 0x811800", when ı debug.

My mcu is mpc5777c.

Could you inform me what can be reason of this issue?

Good works.

0 Kudos
1 Solution
983 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

most probably you have incorrectly set path to source file in you compiler. Try to recompile the code and check the linker and compiler dependencies.

You can also try to manually load the source into your debugger if it supports it. For example for Lauterbach use command, ( y.SourcePATH *)

Best regards,

Peter

View solution in original post

0 Kudos
1 Reply
984 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

most probably you have incorrectly set path to source file in you compiler. Try to recompile the code and check the linker and compiler dependencies.

You can also try to manually load the source into your debugger if it supports it. For example for Lauterbach use command, ( y.SourcePATH *)

Best regards,

Peter

0 Kudos