I would like to implement the BAM MPC5534A
I use a CW for MPC55xx and MPC56xx 2.9 and a MPC5534.
I have created a project using the Project Wizard feature of the Code warrior.
According to the advice of Lukas, I have edited the lcf file for __ start () function is moved to the starting address of SRAM (0x40000000).
Then I have found the problem.
Program entry address offset oxoooo0030
S705400000301A
If I have edited the lcf file for __ start () function is moved to the starting address of SRAM (0x40007000).
S705400070301A
How can I solve this problem?Lukas Zadrapa
And one more thing - be aware there are three errata related to BAM:
http://www.nxp.com/assets/documents/data/en/errata/MPC5534revA.pdf
thank you very much for your help
Why is my application not running, and I'm going to set it up in the bam mode in your way
Thank you very much