Hi,everyone:
I use the S32DS IDE to creat a new project, and use the processor Expert configure the colck,
then i get the Frequence of FLEXCAN1's clock.
when operate the register of CAN1 Module, it will goto INVOR1_Handle.
i check the CAN1 register,it point "buserror"
So, how can i solve this problem, is there has another register need to config or write???
the attachment project is the Test projcet.
Thanks for help!
Hi,thanks for answer, when i set the clock, i switch on SXOSCON in MC_ME_RUN[x]_MC, but on the board not have the 32KHz external oscillator .
i switch off the SXOSCON in MC_ME_RUN[x]_MC, slove this question.
Hi,
I expect that your CAN_1 register MCR bit MDIS is in "1" state.
Could you share with use phycical memory screenshot of dump of CAN MCR. Just to be sure.
Peter