Medium vs Fast I/O Pads

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Medium vs Fast I/O Pads

730件の閲覧回数
bchang32
Contributor III

What is meant by Medium and Fast I/O Pads and what determines each?

 

It appears that the eTPU signals are medium I/O Pads, but is there a way to tell as well as what the diference is? eTPU can go up to 200 MHz. What is the eMIOS pad considered?

 

I'm looking specifically at the MPC5775E.

タグ(1)
0 件の賞賛
返信
1 返信

720件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

According DS terminology, there are following pad types used with MPC5775E:

1. pad_sr_hv = General-purpose I/O pads
- Input specification (DS Table 6)
- Output specification(DS Table 9)

2. pad_ae_hv = Input-only analog pads
- Input specification (DS section 3.8)

3. pad_isatww_st_hv = Input-only pads = Analog and digital input pads
- Input specification (DS section 3.8 and Table 6)

5. pad_sr_hv +MSC = LVDS pads
- Input specification (DS Table 6 and Section 3.10)
- Output specification(DS Table 6 and Section 3.10)

6. pad_sr_hv w/ LFAST = LVDS pads
- Input specification (DS Table 6 and Section 3.10)
- Output specification(DS Table 6 and Section 3.10)

7. pad_fc_hv = EBI pads
- Input specification (DS Table 6, Table 38 for EBI)
- Output specification(DS Table 10, Table 38 for EBI)

I/O Power Domain is specified in the excel sheet MPC5775B_MPC5775E_System_IO_Definition.xlsx (embedded in the RM), column "I/O Power Domain".

VDDEx is considered as I/O supply voltage for fast I/O pads. VDDEHx is considered as I/O supply voltage for medium I/O pads. However medium/fast marking does not make any sense on this device and there are 7 pad typed on this device. It is rather simplified designation.

0 件の賞賛
返信