Maximum baud rate for MPC574x

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Maximum baud rate for MPC574x

544件の閲覧回数
chetkaufman
NXP Employee
NXP Employee

I have a customer looking for 6 UARTs at 10Mbps minimum baud rate.   What is the maximum baud rate for the MPC574x or similar product?

0 件の賞賛
1 返信

433件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello Chet,

I suppose you would like to use MPC574xG/C. For this microcontroller I found following:

pastedImage_1.png

pastedImage_2.png

Maximum frequency is 160MHz = F160, F80 is half of F160 and F40 is half of F80. So if you set F160 fast enough, it should be able to have UART baud rate 10Mbps.

If you have any other questions, please feel free to write me back.

Regards,

Martin

0 件の賞賛