Managing BAF in MPC5777M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Managing BAF in MPC5777M

719 Views
paulodasilvapin
Contributor III

Hello,

With DO178 level A, we need to master all executed code in the platform.

1°) Is it possible to have the source code of the BAF ?

2°) if not, is it possible to overrun the BAF code and run our code defined at our own reset address. Maybe, there is a way to change the SSCM_PSA register ?

3°) Peter Vlna has answered in MPC5777M BAF  that it is possible to erase the BAF sector. If I would like to put our customer boot, how can I do that ?

Thank you

Paulo.

Tags (1)
2 Replies

562 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi again,

I had a chat with system engineer for MPC5777M and he told me that we can share BAF source code.

But it is under NDA agreement. So you have to contact FAE/sales/distributor assigned to your company who will help you sign NDA. If you have already signed NDA then contact person who assisted you with NDA signature.

Peter

562 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

1.) You can dump is from micro. It is written in assembler.

2.) SSCM_PSA is read only register.

pastedImage_1.png

3.) Don't do that. If you erase BAF your micro will be unusable until you load it back.

Peter