I'm trying to use the GetResource example on the peripheral core of the MPC5777M, but I get a compiler error that isync is not available in VLE mode - "Error: Illegal instruction for VLE mode: `isync'"
GetResource:
wrteei 0 # disable external interrupts to the Processor
raise PRI # Write to CPR, cache inhibit, guarded
mbar # flush out writes from store buffer
wrteei 1 # enable external interrupts to the Processor
isync # re-fetch Processor pipeline
Is there a way to build in bookE mode for the e200z4 on the 77M? Or is there a different instruction I should be using to force instruction sync?
Thanks,
Jacob
EDIT, did more research:
Is the correct instruction se_isync?
已解决! 转到解答。