MPC5777M peripheral core isync

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5777M peripheral core isync

ソリューションへジャンプ
1,962件の閲覧回数
jschloss
Contributor III

I'm trying to use the GetResource example on the peripheral core of the MPC5777M, but I get a compiler error that isync is not available in VLE mode - "Error: Illegal instruction for VLE mode: `isync'"

GetResource:
wrteei 0 # disable external interrupts to the Processor
raise PRI # Write to CPR, cache inhibit, guarded
mbar # flush out writes from store buffer
wrteei 1 # enable external interrupts to the Processor
isync # re-fetch Processor pipeline

Is there a way to build in bookE mode for the e200z4 on the 77M? Or is there a different instruction I should be using to force instruction sync?

Thanks,

Jacob

EDIT, did more research:

Is the correct instruction se_isync?

タグ(3)
0 件の賞賛
返信
1 解決策
1,823件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, se_isync is correct syntax.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,824件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, se_isync is correct syntax.

0 件の賞賛
返信