MPC5777M I/O 416 BGA package

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777M I/O 416 BGA package

541 Views
MP
Contributor I

Hi,

i would like to supply VDD_HV_IO_MAIN with 3.3V.

I have read several threads about this issue, e.g. this one https://community.nxp.com/t5/MPC5xxx/CAN-MPC5777M-VDD-HV-IO-MIAN-connect-to-3-3V/m-p/1212784

There @davidtosenovjan wrote, that it can be, but with limitations. With the limitations that the flash memory is only used in read-only mode.

I understand that you have to disable LVD400, but why do I have limitations with the 416 BGA package? VDD_HV_PMC has a separate supply pin that can be supplied with 5V. As far as i understand it, i would not have limitations. Is that correct?

 

0 Kudos
Reply
1 Reply

532 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, yes you are right. With 416BGA package, you may use separate voltage for VDD_HV_PMC. Low voltage detector VLVD400 must be disabled anyway, as it is related VDD_HV_IO_MAIN segment. And not only this one but apparently others as well.

davidtosenovjan_1-1629721323900.png

davidtosenovjan_2-1629721427919.png

 

 

 

0 Kudos
Reply