MPC5777M EBI for external flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777M EBI for external flash

676 Views
bwp530
Contributor IV

I found two external flash on EVB, I want some example to test it. 

Tags (2)
0 Kudos
2 Replies

520 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi,

there are two ways how external flash is being used

1) either you want to execute compiled code (possibly boot from the external flash)

2) or you want to read and program the data during runtime by user application

 

Case 1)

Usually you would use standalone programmer like PeMicro Cyclone MAX, or other that is capable to program specified .elf file directly to external memory device connected to MCU with using specific programming algorithm delivered by programmer manufacturer. For instance, following one

http://www.pemicro.com/cyclone/index.cfm

 

Of course, other third-party programmer’s providers exist.

 

Case 2)

User can write his own flash programming driver according to sequence of commands over EBI address and data lines according to sequence described if specific memory’s datasheet.

Unfortunately, currently I don't have example code I could share with you.

0 Kudos

520 Views
bwp530
Contributor IV

davidtosenovjan‌  I have made a code of external flash on EVB board, but when I debug the code on EVB, the program will crash once it accesses the 0x20000000. I am confused about this. 

uint16_t i = 0;

SIUL2.MSCR_IO[289].R = 0x32000003u;
SIUL2.MSCR_IO[290].R = 0x32010003u;
SIUL2.MSCR_IO[291].R = 0x32390003u;
SIUL2.MSCR_IO[292].R = 0x32000003u;
SIUL2.MSCR_IO[293].R = 0x32000003u;
SIUL2.MSCR_IO[294].R = 0x32000003u;
SIUL2.MSCR_IO[295].R = 0x32010002u;
SIUL2.MSCR_IO[296].R = 0x32390003u;

for(i=297; i<321; i++){
SIUL2.MSCR_IO[i].R = 0x32000003u;

}

/* PS0-15 PT0-15*/
for(i=257; i<289; i++){
SIUL2.MSCR_IO[i].R = 0x32380003u;
}

/* Base Address: 0x20000000, 32-bit, Mux'd bus */
EBI.BR0.R = 0x20000083;
EBI.BR1.R = 0x21000083;


/* Address Mask: 512KBytes, One Wait States - Pipelined Sync SRAM */
EBI.OR0.R = 0xFF000010;
EBI.OR1.R = 0xFF000010;

/* MCR - 16-bit mode */
EBI.MCR.R = 0x00000000;

if I use EBI, what reason can make the program can't access the address and crash. Is there anything else to configure? like ld file or something.

1.png

0 Kudos