MPC5777C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5777C

727 次查看
PENGHAN
Contributor II

 

Hello,The chip I use is mpc5777C, the IDE is S32DS2.1, and the program is added in the attachment. When I debug the Decrementer interrupt (interrupt number 10), the program will run away.
Proceed as follows:
First initialize the HID0 register, TSR, TCR register;
Then initialize IVPR and IVOR10;
Finally, the program will jump to IVOR10_Handler;
Please help me solve how the program jumps to interrupt No. 10 and executes related functions.

Respect

0 项奖励
2 回复数

693 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I did some changes so project can be compiled and goes to you int_dec_isr interrupt.

BR, Petr

0 项奖励

328 次查看
kaffel
Contributor I

Hi,

I built the MPC5777C_DSPI_Master_TXRX_DMA_S32DSPower21_Z7_0 project, I connected the SDO and SDI(loopback), I ran the code to see the  DSPI_Master_Receive_Data is not udpated it always 0 any idea?, i can see the sck and SDO dataout on the scope.

 

Thanks
Mohamed.

0 项奖励