MPC5777C two eqadc module can work at the same time?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C two eqadc module can work at the same time?

1,148 Views
Alex5080
Contributor II

MPC5777C has two hardware eqadc module. To  speed sample time and collect data. I hope that  two moduel can work at the same time in parallel.   would you help to provide reference example?

0 Kudos
6 Replies

1,072 Views
Alex5080
Contributor II

anyone can help to check this case?

0 Kudos

1,091 Views
Alex5080
Contributor II

hello,  I find that those example only run one eQADC module(2 ADC units).   would you please share the example which run 2 eQADC modules(4 ADC units).?

Attached file is our file,  it canot work well.    we need close 1 eQADC modules, then run another  eQADC moduels. .we find these 2 eQADC moduels doesn't work at the same time.

0 Kudos

1,023 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport
0 Kudos

1,075 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I am attaching previous version (v0_2) of the example where I have been using eQADC_B, v0_3 has been changed to eQADC_A. You could combine it together.

Tags (1)
0 Kudos

1,063 Views
Alex5080
Contributor II

after combined v02/v03,  two resultis is zero.

0 Kudos

1,137 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

There are 2 eQADC modules on this device, both consists of 2 ADC units => you may convert 4 channels in parallel, but it must be different channels.

Example codes you may find here, browse for eQADC:

https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445

 

0 Kudos