MPC5777C has two hardware eqadc module. To speed sample time and collect data. I hope that two moduel can work at the same time in parallel. would you help to provide reference example?
anyone can help to check this case?
hello, I find that those example only run one eQADC module(2 ADC units). would you please share the example which run 2 eQADC modules(4 ADC units).?
Attached file is our file, it canot work well. we need close 1 eQADC modules, then run another eQADC moduels. .we find these 2 eQADC moduels doesn't work at the same time.
I made the example. It works fine. Here is the link:
I am attaching previous version (v0_2) of the example where I have been using eQADC_B, v0_3 has been changed to eQADC_A. You could combine it together.
There are 2 eQADC modules on this device, both consists of 2 ADC units => you may convert 4 channels in parallel, but it must be different channels.
Example codes you may find here, browse for eQADC:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445