MPC5777C problems to Transmit and receive data with Host Computer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C problems to Transmit and receive data with Host Computer

658 Views
thiagoduarte
Contributor II

Hi. 

I am using a MPC5777C with a MPC57XX Motherboard Rev C.

I tried to configure the FEC using the last configuration indicated on  Questions of MPC5777C FEC setting

The microcontroller is transmitting a simple packet and ARP request packets too.

Using the wireshark, with the ETH board in promiscuous mode , the data cannot be received.

The micro controller receive wrongly the packets generated by the host computer ( size and type )

 

When I used the loopback indicated on post Problems about receiving ethernet frame on MPC5604E  the microcontroller could receive the ARP packets transmitted. 

The clock configuration is the same as Example MPC5777C-PinToggleStationery GHS714 

I am using a MPC57xx MB Rev C,

The Jumper Configuration

J26 is 1-2.

J510 is 1-2.

J514 is 2-3.

Is there any other missing configuration can cause its problem ?

It is possible share any example like Need sample code MPC5777M Fast Ethernet Controller to communicate TJA1100 NXP PHY  for MPC5777C using the PHY of the motherboard?

Thanks.

0 Kudos
0 Replies