MPC5777C M_CAN0 problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5777C M_CAN0 problem

624 Views
markus_fischer1
Contributor II

Hallo,

is there any application note like AN5045 (MPC5777M) for the processor (MPC5777C)? There are main differents between this both CPU´s so i can not use this as example.

I try to use the example https://community.nxp.com/docs/DOC-332736 . But in this examplere are used a other IDE, so this won't work well. So I try to Change this example to use with the S32 IDE and i can not send or recieve any can Messages. 

IDE: S32 Design Studio for Power Architecture

Debugger: PE Micro Multilink Universal FX

Can: 0

I try to recieve an package and send the same package back. So after recieve a message not work, i try to send only a message, but there are any wrong in my Code.

Tags (3)
0 Kudos
1 Reply

462 Views
markus_fischer1
Contributor II

i try to convert this Project again, and this work.

0 Kudos