MPC5777C JTAG minimum signals

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5777C JTAG minimum signals

跳至解决方案
4,564 次查看
EAlepins
Contributor V

What is the minimum JTAG signals that should be routed to my JTAG connector for the MPC5777C debugging to work properly?

Thanks.

Étienne

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
4,191 次查看
randyd
NXP Employee
NXP Employee

TDI, TDO, TMS, TCK, RESET, JTAG Supply voltage reference (VREF), and ground.

JCOMP depends on the debugger that you are using. Some debuggers allow the JCOMP to be pull high on the board and not connected to the JTAG connector. They include a command to override the debugger having to drive the signal. However, some debugger do not include this functionality. You should check with your debugger supplier. 

RDY and EVTI are optional signals. RDY allows for faster block moves over the JTAG interface. This can be beneficial during flash programming. 

See the MPC5777C Hardware requirements application note:

https://www.nxp.com/docs/en/application-note/AN5268.pdf 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,192 次查看
randyd
NXP Employee
NXP Employee

TDI, TDO, TMS, TCK, RESET, JTAG Supply voltage reference (VREF), and ground.

JCOMP depends on the debugger that you are using. Some debuggers allow the JCOMP to be pull high on the board and not connected to the JTAG connector. They include a command to override the debugger having to drive the signal. However, some debugger do not include this functionality. You should check with your debugger supplier. 

RDY and EVTI are optional signals. RDY allows for faster block moves over the JTAG interface. This can be beneficial during flash programming. 

See the MPC5777C Hardware requirements application note:

https://www.nxp.com/docs/en/application-note/AN5268.pdf 

0 项奖励
回复
4,191 次查看
EAlepins
Contributor V

Please answer...

0 项奖励
回复